Open an object

Open an object from
Project view
.
  • In
    Project view
    , double-click the object or mouse over the object and then select
    Editor
    .
The object opens in a separate tab if the object has a dedicated editor.
Properties
for the object also open.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal