View node references

View references to display all of the objects in the information model that reference a node.
  1. In
    Project view
    , right-click the node or item and then select
    Show References
    .
  2. In
    References of (name)
    , select a location and then select
    Go to ...
FactoryTalk Optix Studio
navigates to the instance of the type. Objects referenced in a NetLogic are not shown.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal