Certificates and keys location

The certificates and keys are organized in this folder structure.

Certificates and keys in projects

ProjectFiles/PKI/
  • Own
    • Certs
      . Allowed application certificates.
    • Crl
      . Revoked application certificates.
  • Trusted
    • Certs
      . Allowed certificates of trusted remote applications.
    • Crl
      . Revoked certificates of trusted remote applications.
  • Issuers
    • Certs
      . Allowed certificate authority (CA) certificates.
    • Crl
      . Revoked CA certificates.

Certificates and keys in runtime applications

ApplicationFiles/PKI/
  • Trusted
    • Certs
      . Allowed certificates of trusted remote applications.
    • Crl
      . Revoked certificates of trusted remote applications.
  • Issuers
    • Certs
      . Allowed certificate authority (CA) certificates.
    • Crl
      . Revoked CA certificates.
  • Rejected
    . Rejected certificates of remote applications that are not trusted.
TIP: To enable certificates management at runtime, certificates from the
ProjectFiles/PKI/
folder are copied to the
ApplicationFiles/PKI/
folder with the
internal_
prefix when you start the
FactoryTalk Optix Application
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal