Configure Custom Payload
    - In Project View, select the MQTT Publisher you want to modify.
- In the properties, underPayload formatter:- SetPF EnabledtoTrue.Payload Formatter is enabled.
- Next to thePF Header, select the dynamic link.
- In the new window, in theAdvancedtab, define the header string format, and selectCreate.
- Next to thePF Record, select the dynamic link.
- In the new window, in theAdvancedtab, define the record string format, and selectCreate.TIP: If you do not have any records, you can leave thePF Recordblank.
 
Provide Feedback