Delete an event logger

Delete an event logger by removing the event logger object in
Project view
.
TIP: You can disable an event logger without the need to completely remove the logger from the project. For more information, see Edit an event logger.
  • In
    Project view
    , right-click an event logger object and select
    Delete
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal