Add a widget to a project

You can add preconfigured widgets to a project. Use widgets to configure the FactoryTalk Optix Application at runtime, configure the device on which the application is running, and show information about the device.
NOTE: An
OptixPanel
project contains
Date & Time
,
Device
,
Network
, and
FT Remote Access
widgets in the
Project view
by default.
  1. From the main toolbar, select
    Libraries
    .
  2. In
    Libraries
    , select
    Widgets
    .
  3. Select the widget to add to the project.
  4. Under
    Components
    , complete the instructions to add the widget to the project.
  5. When the widget is added, in
    Libraries
    , select
    Close
    .
The widget appears in
Project view
.
TIP: If you add a widget that contains a node with the same name as the node that already exists in the project, the dynamic links are remapped to the node that exists in the project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal