Commit a library

Commit changes to a local or remote library to save changes on the local computer only. Committed changes are not backed up (or pushed) to a remote repository.
  1. To commit a library
  2. From the main toolbar, select
    Template Libraries
    .
  3. Select
    Commit
    .
  4. Enter a meaningful commit message.
  5. Select
    OK
    .
A new version of the library is saved on the local computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal