Configure an image
Add an image object and edit its properties.
- InProject view, inUI, right-click a container to contain the image, and then select .
- Select the image to include:
- InProperties, next toPath, selectBrowseand select an image to include into your application.
- On the canvas, double-click
and select an image to include into your application.
TIP:To find items, start typing the item name to find inSelect file.If the file does not appear inSelect file, selectand inImport file(s)Import file(s), select the file to import and then chooseSelect. - (optional) InProperties, set the image appearance:
- Visible. Show the image at runtime.
- Enabled. Enable interaction with the image at runtime.
- Opacity. Set the image opacity level (in percentages).
- Blink. Blink the image at runtime.
- Rotation. Rotate the image around its center point (in arc degrees). Positive values rotate the image clockwise; Negative values rotate the image counterclockwise.
- Dynamic color. Only for SVG images format. Colorize the image with the selected color.
- Colorization mode. Set the colorization mode of the image forDynamic color.
- Hit test visible. Intercept user selections. False by default - user selections are not intercepted and are passed to the underlying object.
- Fill mode. Select either:
- Fit. The image keeps its original aspect ration when resized.
- Stretch. The image fills the container and ignores its original aspect ratio when resized.
- Move target. See Make a graphic object movable.
- (optional) To resize, move, or align the image, see Graphic objects layout.
- (optional) InProperties, set image margins (nine slicling):TIP:Setting image margins prevents distortions in the peripheral sections of an image when resizing.For example, you implement an image that has a black border. By setting image margins, you can make the black border not react to image size changes.
- Image left margin. Size of the left peripheral section of the image to exclude when resizing the image.
- Image top margin. Size of the top peripheral section of the image to exclude when resizing the image.
- Image right margin. Size of the right peripheral section of the image to exclude when resizing the image.
- Image bottom margin. Size of the bottom peripheral section of the image to exclude when resizing the image.
image
nine slicling
nineslicing
slicing
Provide Feedback