Drawings

Use drawings objects to add shapes and images to your application interface.
Object
Description
A rectangle or square that displays at runtime. Use rectangles to create buttons or group other relevant objects. See Draw a rectangle or square.
An ellipse or circle that displays at runtime. Use ellipses to create buttons or group other relevant objects. See Draw an oval or circle.
A
PNG
,
JPG
,
JPEG
,
BMP
, or
SVG
image. For example, a logo.
An object that can have multiple image states based on the input value. Each image state may reference a different image and may have a specific opacity. If the input value does not correspond with any image state, the default value is used (first defined state).
An SVG Tiny 1.2 image, which properties of individual image parts can be changed at design time or runtime. For example, an alarm may trigger a particular part of an image to become red.
Line
A line you can draw and for which you can customize the appearance. See Draw a line.
Polyline
A polyline and polygon that can be selected at runtime and for which you can customize the appearance. See Draw a polyline or polygon.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal