Zoom in and zoom out a trend chart

Zoom the X and Y axes of a trend chart to focus on specific data. Zoom in and out the trend chart axes together or separately. Zooming applies only to the
Normal
and
Time range
trend modes.
  • To zoom the trend chart:
    • Use the pinch-to-zoom gesture.
    • Place the mouse pointer in the area of interest of the trend chart and scroll forward or backward.
    • Select the trend chart and select
      +
      or
      -
      .
  • To zoom the X-axis only, place the mouse pointer anywhere in the trend chart, hold
    , and then scroll up or down.
  • To zoom the Y-axis only, place the mouse pointer anywhere in the trend chart, hold
    , and then scroll up or down.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal