Configure a sparkline
    Configure the source of the data to display in the Sparkline object. Adjust the Sparkline object properties.
     IMPORTANT: 
    Do not use polylines as containers for sparklines.
- InProject view, right-click a node to contain theSparklineobject and select .
- InProperties, either:- Create a dynamic link between thePen valueproperty and a project node. This obtains values of attributes or properties of all direct child nodes.For example, select aModelfolder with objects that contain data. For more information, see Project nodes
- Create a dynamic link between thePen valueproperty and a database object. This obtains data contained in database tables.For example, select an Embedded, ODBC, or InfluxDB database object. For more information, see Database.
 For more information about dynamic links, see Create dynamic links.
- (optional) Configure the sparkline properties:- Pen color. Sparkline pen color.
- Pen thickness. Sparkline pen thickness.
- Time window. Sparkline time range.
- Refresh time. Sparkline refresh time.
- Y-axis maximum. Maximum value of the Y-axis.
- Y-axis minimum. Minimum value of the Y-axis.
- Range high. High value of the range.
- Range low. Low value of the range.
- Range color. Range background color.
 
sparkline
    
Provide Feedback