Configure a Histogram chart

Configure a
Histogram chart
object to get data from a project node or a database.
  1. In
    Project view
    , in
    UI
    , right-click a container and then select
    New
    Data controls
    Histogram chart
    .
  2. In
    Properties
    , either:
    • Create a dynamic link between the
      Model
      property and a project node. This obtains values of attributes or properties of all direct child nodes.
      For example, select the
      Model
      folder with objects that contain data. For more information, see Project nodes.
    • Create a dynamic link between the
      Model
      property and a database object. This obtains data contained in database tables.
      For example, select an Embedded, ODBC, or InfluxDB database object. For more information, see Database.
    For more information about dynamic links, see Create dynamic links.
  3. (optional) Specify the kind of items to display in the object by setting
    ItemKind
    .
    TIP:
    The
    ItemKind
    property is automatically set with the object or variable type recognized among the child nodes.
    For example, if the model is based on a folder node that contains several instances of a
    Motor
    object type,
    ItemKind
    is automatically set with the reference to the
    Motor
    type. In this case, the values that display are the attributes or properties of different instances (
    Motor1
    ,
    Motor2
    ,
    Motor3
    , and so on).
  4. (optional) In
    Query
    , enter a standard SQL query to filter items obtained from a database or project nodes as specified in
    Model
    .
    For more information, see SQL queries.
    For example:
    SELECT * FROM Model WHERE SPEED > 40
    SELECT * FROM "DataLogger1" WHERE Speed > 40
  5. Configure chart labels by creating a dynamic link between
    Label
    and a variable argument such as
    @BrowseName
    .
  6. (optional) In
    Value
    create a dynamic link between a relevant property value.
    For more information about dynamic links, see Create dynamic links.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal