Configure a video

Insert a video file container to your project, and place a video file in it. Use video files local to the project or remote videos.
  1. In
    Project view
    , in
    UI
    , right-click a container and then select
    New
    Contents
    Video
    .
  2. In
    Path
    , either:
    • Select
      Browse
      and select the local video to display.
      TIP:
      To find items, start typing the item name to find in
      Select file
      .
      If the file does not appear in
      Select file
      , select
      Import file(s)
      and in
      Import file(s)
      , select the file to import and then choose
      Select
      .
    • Enter the address of the remote video file to display.
  3. (optional) Set the auto play options.
    • Auto play
      . Video will be played automatically. Disabled by default.
    • Muted
      . Video will play without sound. Disabled by default.
    • Loops
      . Specifies the number of times video will play. The default is
      1
      .
  4. (optional)
    Muted
    .
  5. (optional) Set the
    Appearance
    and
    Size and layout
    properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal