Configure a navigation panel
    Configure a navigation panel by referencing panel objects as tabs.
- InProject view, inUI, right-click a container and select .
- InProject view, double-click the navigation panel.Navigation panel displays in the editor.
- CreatePaneltypes that you want to reference as tabs in the navigation panel.For more information, see Create a graphic object type.
- FromProject view, drag the panel types onto the navigation panel in the editor.As you drop panel types onto the navigation panel in the editor, the preview of the first panel and navigation tabs display. InProperties,Panelpopulates automatically.
- (optional) InProperties, create a dynamic link betweenCurrent tab indexand the application logic that governs the currently selected tab.For more information about dynamic links, see Create dynamic links.TIP: The tab index starts with and defaults to 0. The 0 index value indicates the first tab.
- (optional) InProperties, underPanel#, set properties for each navigation panel tab:- Title. Title of the navigation panel tab.
- Image path. Path to the image that overrides the panel title. For seamless integration of the image with the UI, use correctly sized flat images with a transparent background.
- Enabled. Allows interaction with the tab on the device. Defaults to True.
- Visible. Makes the tab visible. Defaults to True.
 
- (optional) InProperties, inAttached panel loader, create a dynamic link to the panel loader to attach.For more information about dynamic links, see Create dynamic links.TIP: Attaching a panel loader displays the contents of navigation panel tabs in the panel loader.
- (optional) UnderAppearance, set the panel properties:- Visible. Makes the panel visible. Defaults to True.
- Enabled. Allows interaction with the panel on the device. Defaults to True.
- Opacity. Sets the opacity of the panel. Defaults to 100, which means no opacity.
- Rotation. Rotates the panel around its center point. Positive values rotate the panel clockwise.
- Move target. Makes the panel movable at runtime. For more information, see Make a graphic object movable.
- Tab position. Determines the position of panel tabs or hides the tabs.
- Tab width. Tab width in pixels.
- Tab height. Tab height in pixels.
- Appearance. Navigation panel appearance.
- Style. Navigation panel graphic style. For more information, see Style sheets.
 
navigation
navigation panel
    
Provide Feedback