Configure a momentary button
    - InProject view, right-click a node to contain the button and select .For example, add the button underMainWindow (type).
- (optional) InProject view, hover-over the button, select, and enter a new name for the button. 
- (optional) InProperties, adjust the button look and feel:- Appearance. Adjust the button visibility, state, opacity, rotation, background color, and style.
- Size and layout. Adjust the button size and position in your project.
- Text and font. Enter the text to display in the button and adjust the text style.
- Image. Include an icon inside the button and decide where to place the icon in relation to the button text.TIP: SelectBrowseand then either selectto add an image to the project or select an existing image in the project. Set Import file(s)Image positionto align the image in relation to the button text. Import file(s)Image positionto align the image in relation to the button text.
 
- InEvents, create dynamic links between specific events and methods to execute.For more information about the available events, see Momentary button.
momentary
momentary button
    
Provide Feedback