Enable or disable a graphic object

Enable or disable an object. At runtime, users can interact with enabled objects.
  1. In
    Project view
    or in the editor, select the object to enable.
  2. In
    Properties
    , in
    Enabled
    , select either:
    • True
      . The object allows user interaction at runtime.
    • False
      . The object prevents user interaction at runtime.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal