Delete a graphic object

Delete a graphic object to remove the object from the project.
  • In
    Project view
    or in the editor, right-click the object to delete and select
    Delete
    .
    TIP: You can also select the object to delete and press
    .
The object is removed from the project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal