Change graphic object visibility

Determine whether an object is visible at runtime.
  1. In the
    Project view
    or in the editor, select an object.
  2. In
    Properties
    , in
    Visible
    , select either:
    • True
      . The object appears in the window at runtime.
    • False
      . The object does not appear in the window at runtime.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal