Set margins

Edit the space around an object.
Prerequisites
  1. To edit object margins
  2. In
    Project view
    , select the object to edit.
  3. In
    Margin
    properties, enter the value for the space between the edge of the parent object that contains the object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal