FTP

File Transfer Protocol (FTP) is used to communicate and transfer files between computers that are on a Transmission Control Protocol/Internet Protocol (TCP/IP) network.
To establish and communicate on the network, an FTP connection requires a server and a client. The following section describes the configuration of these two elements.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal