Delete an event

Delete a an event to no longer have that event to no longer have the event in the project. The event methods are removed along with the event.
  1. Delete all of the methods from an event to delete the event. In
    Project view
    , select an object. In
    Properties
    under
    Events
    , expand the event.  After the method to delete, select
    Delete
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal