Remove a dynamic link

Remove a dynamic link from a property to no longer have the property display the linked attribute. After removing the dynamic link you can reset the default value for the property.
Prerequisites
  1. To remove a dynamic link
  2. In
    Project view
    or the editor, select the graphic object that contains the property with the dynamic link.
  3. In
    Properties
    , in the property that contains the dynamic link, right-click the dynamic link and select
    Remove link
    .
    The dynamic link is removed from the property and the value entered for the property appears.
  4. (optional) Right-click the property value and select
    Reset value
    .
    The property displays its default value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal