Edit a dynamic link

Edit a dynamic link to change the source variable or resolve a broken or unresolved link. Insert a placeholder such as {0} to make the link dynamic. Broken links display in the property while unresolved links display . Unresolved dynamic links cannot be resolved at design time, but they can be valid at runtime, for example, when setting a dynamic link that passes through a panel loader.
Edit a dynamic link by either editing the link manually, selecting a new source, or dragging a new source to the dynamic link in
Properties
.
  • To edit the dynamic link manually:
    1. In
      Properties
      , hover over a dynamic link and select
      Edit
      .
    2. Edit the path and then press
      .
      TIP: You can edit Alias indexes.
  • To edit the dynamic link by selecting a new source:
    1. In
      Properties
      , in the property with the dynamic link, select either the link in the property or select
      Change Dynamic Link
      .
    2. In the dynamic link browser, select a node to act as the source of the value property.
    3. (optional) In
      Attribute
      , select the OPC UA attribute to apply to the selected node. For example, select
      BrowseName
      ,
      Value
      , or
      DisplayName
      .
    4. (optional) In
      Format
      , select the format to apply to the selected variable.
    5. (optional) In
      Array index
      , select the array index of the selected variable. This option appears for array variables only.
    6. In
      Bit index
      , select the index to access the specified bit of the selected variable.
    7. (optional) To create a complex dynamic link, select
      Advanced
      .
      NOTE: For more information, see Create a complex dynamic link.
    8. Choose
      Select
      .
  • To edit the dynamic link by dragging a new source, drag the new source onto the existing dynamic link in
    Properties
    .
  • To restore a dynamic link for which you have selected the variable, right-click the property value and then select
    Restore link
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal