Synchronize imported tags

Synchronize imported tags to update their data types, names, and structures.
  1. To synchronize imported tags
  2. In
    Project view
    , under a
    Communication station
    , double-click
    TagImporter
    .
    The editor opens in a separate tab and displays the status of each controller tag in the project.
    Crossed out tags with red background may display if you:
    TIP: If you import FactoryTalk Design Studio tags offline, any routine scoped tags are imported and referenced in the FactoryTalk Optix Application. However, if you then deploy the FactoryTalk Design Studio project through Logix Designer, any routine scoped tags are not deployed or downloaded to the controller because Logix Designer does not support routine scoped tags. Therefore, if you deploy that FactoryTalk Optix Application to a runtime device and connect the application to the controller, the routine scoped tag references display an error at runtime because the tags were not downloaded to the controller.
  3. Make any necessary edits to the tags.
  4. Select
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal