Set dynamic variables polling time for controllers

Set the time interval between readings of tag values from controllers at runtime.
  1. In
    Project view
    , select
    NativePresentationEngine
    or
    WebPresentationEngine
    .
    For more information, see Presentation engines.
  2. In
    Properties
    , set
    Dynamic variables polling time
    .
    TIP: Set the polling time between one sampling and the next in HHHH:MM:SS.MS format.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal