Create an instance of a tag type

When you import tag types, you can create instances of those tag types in the project.
Prerequisites
Import tag types from a controller. See Configure a communication driver.
  1. To create an instance of a tag type
  2. In
    Project view
    , right-click the
    Model
    folder or its subfolder.
  3. Select
    New
    Tag structures
    StationName
    TagTypeToInstantiate
    .
Tag instances display in the project model. Any synchronized changes to the imported tag types are reflected in these tag instances.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal