Shelve and unshelve alarms

Shelve and unshelve alarms at runtime. Shelving alarms prevents the notification of new state changes. Shelve duration is assigned to the alarm in the project.
  1. At runtime, in the
    Alarm manager
    , select the alarm to modify.
  2. Perform one of the following actions:
    • To timed shelve the alarm, select
      Timed-Shelve
      , select the shelve duration, and select
      Shelve
      .
    • To one-shot Shelve the alarm, select
      One-Shot Shelve
      .
    • To unshelve the alarm, select
      Unshelve
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal