Set dynamic variables polling time for alarms

Set the time interval between readings of variable values from OPC UA servers and tag values from controllers.
  1. In
    Project view
    , select the root project node.
  2. In
    Properties
    , set
    Dynamic variables polling time
    .
    TIP: Set the polling time between one sampling and the next in HHHH:MM:SS.MS format.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal