Automatically confirm and acknowledge alarms

Reduce the interaction required to manage alarms at runtime. Have the application confirm and acknowledge alarms automatically.
  1. In
    Project view
    , select the
    Alarm grid
    .
  2. In
    Properties
    , configure:
    • Auto confirm
      . Select
      True
      to confirm that the issues causing alarms are resolved at runtime automatically. The
      Alarm grid
      displays only active and unacknowledged alarms.
    • Auto acknowledge
      . Select
      True
      to acknowledge alarms at runtime automatically. The
      Alarm grid
      displays only active and unconfirmed alarms.
      TIP: To have the
      Alarm grid
      display only active alarms at runtime, in
      Properties
      for the grid, set both
      Auto confirm
      and
      Auto acknowledge
      to
      True
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal