Getting Started with FactoryTalk Hub
FactoryTalk Hub is the online location where you can access Rockwell Automation's cloud-based Software as a Service (SaaS) offerings to simplify the way you design, create, and maintain your assets.
NOTE:
This section of the help contains information needed to get started with FactoryTalk Hub. See Entitlements for information on Entitlements and Universal Credits, and Manage Your Organization for more information on managing your organizations after you create them.
To get started with FactoryTalk Hub, you must:
- Browse to and sign in to FactoryTalk Hub.
NOTE:
The organization you belong to controls the services available to you in FactoryTalk Hub.
Authentication
FactoryTalk Hub uses your MyRockwell user profile to authenticate your access and determine your organization. You can be a member of more than one organization.
After your account has been authenticated, your browser displays the FactoryTalk Hub
Home
screen. Panels will be displayed that identify the services entitled for your use.The organizational administrator can use the
Hub Menu
at the upper left of the page to manage user access, view entitlements, invite users, approve users, and manage organization invites. The Organization section of the Hub Menu allows you to create, edit, or join organizations, as well as view your Universal Credits Balance.
TIP:
If the link isn't visible, you are not logged in as an organization administrator.
To open a service
Click the
title
for the service, such as FactoryTalk Design Studio or FactoryTalk Remote Access, to go to that service.Click
Home
to return to the Home screen.Each service has Getting Started information in the online help to help you learn how to perform different tasks.
FactoryTalk Hub Home Page
The following image shows the parts of the FactoryTalk Hub home page.
FactoryTalk Hub Home Page

Callout | Item |
---|---|
1 | FactoryTalk Hub Menu. Contains Hub Manager and Organization menus. |
2 | Name of the FactoryTalk Hub service you are currently using. |
3 | FactoryTalk Hub Service tiles area. Allows you to select and launch services you are entitled to use. By selecting the star on an application tile, you mark it as a favorite and the tile appears with the other favorites in the favorites row. |
4 | The organization you are working with. |
5 | Notifications menu. Select to see notifications that have been sent to your organization. A red number here indicates the number of unread notifications that you have waiting. |
6 | Help button. Provides access to the help menu for the current application. On the main FactoryTalk Hub screen, this link goes to FactoryTalk Hub help. Otherwise to help for the application you are using. |
7 | Access the profile of the current user. |
FactoryTalk Hub tiles are arranged by sections that only appear if you have access to an application that would be in that section. For example, if you have not made any applications favorites you do not see a favorites section. There is also information and interactivity associated with each tile.
FactoryTalk Hub Tiles and Badges

Tile Type or Badge | Description | Notes |
---|---|---|
Tile Sections: | ||
Pending for (Org Name) | Tiles for not provisioned services and for which the logged in user is an Admin or Owner for the organization and has active unallocated entitlements for the service. | This section only appears for administrators and owners of the organization. |
Favorites | Tiles marked by the user as Favorites. | |
For you | Displays the tiles for applications that are already provisioned for the organization, and the user has access and can open them. | |
By request | Displays the tiles for applications that are provisioned for the organization but the user does not have access to them and cannot open them. The user must request access from the administrator. | |
More from Rockwell Automation | Displays the rest of tiles for all other applications available in FactoryTalk Hub that are not provisioned for the organization or are available for preview only. | |
Icon on tiles: | ||
Star on tile | A filled star indicates that the user has marked it as a favorite. Once marked, the tile will also appear in the favorites section of FactoryTalk Hub. | The star appears empty if the application is not selected as a Favorite |
Purple icon with number inside | Indicates the number of entitlements the user has available to allocate for that service. | Only appears to Admins or Owners of the organization. |
Red icon with exclamation point inside |
| Only appears to Admins or Owners of the organization. The purple icon cannot appear when this icon is displayed. |
Action buttons on tiles: | ||
Add+ | Opens View Entitlements screen. | Appears when the logged in user is an Admin or Owner for the organization and has active, unallocated entitlements for the service. |
Open | Opens the application in a new tab | |
Product info | Opens a a pop-up with the product description | |
Set up | Opens the application to complete provisioning workflow. | The logged in user must be an Admin or Owner of the organization. |
Provide Feedback