Provide feedback

Operations Hub includes an option for the User to provide feedback about their experience with the service to the FactoryTalk Hub team. Follow these steps to provide feedback:
  1. Navigate to the top banner and click the question mark (
    ?
    ) icon. A list of help options displays.
  2. Click
    Provide Feedback.
    The
    Feedback
    dialog box displays.
  3. Select a feedback topic from the pull-down list. The available options are:
    • Provide Feedback
    • Enhancement Request
    • Report an Issue
  4. Enter the details of your feedback, request, or issue into the space provided. A maximum of 1000 characters is permitted.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal