Welcome
The Welcome screen in
FactoryTalk Design Studio
is the first screen that you see when you launch the software. It provides quick access to various features and functions of the software. Here are some of the key features of the Welcome screen. - Open project. Open a project that you have previously created and saved inFactoryTalk Design Studio.
- New project. Create a project from scratch.
- Recent Projects. List of projects that you recently opened or worked on. Select a project from the list to access the project quickly.
- Help. Opens theFactoryTalk Design Studioonline help. TheFactoryTalk Design Studioonline help provides help topics to assist you in learning about the features and capabilities inFactoryTalk Design Studio.
- Getting started. Accessed from the
Help on the top right of the application, the
Getting startedpage provides a brief description and links to information about the features that you should use to get started inFactoryTalk Design Studio. TheGetting startedpage gives an overview of designing your system, reusing content, collaborating with other users through version control, and getting your system ready for production using the FactoryTalk Vault.
The Welcome screen opens by default when you launch
and then
FactoryTalk Design Studio
. Return to the Welcome screen any time by selecting 
Welcome
.Provide Feedback