View a device profile

View a device profile to view and edit device settings such as connections, ports, and electronic keying.
TIP: If you are online, the profile will open in read-only. You can use the offline icon to open the offline version of the profile.
  1. On the explorer bar, select Devices Icon
    Devices
    .
  2. In
    Devices
    , select
    Device list
    .
  3. In
    Device list
    , right-click the device, then select
    Open device properties
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal