Add a rung comment

Add a rung comment to describe the tasks that the rung performs in the routine.
Prerequisites
To add a rung comment
  1. Right-click the rung and select
    Add rung comment
    .
  2. In
    Rung comment
    , type the rung comment.
  3. Select
    Accept
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal