Remove a parameter from an instruction

Remove an input or return parameter to no longer have the parameter in the instruction. You can remove a parameter from a Jump to Subroutine (JSR), Subroutine (SBR), or Return (RET) instruction.
Prerequisites
To remove a parameter from an instruction
  • In the JSR, SBR, or RET instruction, right-click the parameter to remove and then select
    Remove Instruction Parameter
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal