Move a ladder diagram instruction

Move a ladder diagram instruction in a ladder diagram routine to have the instruction execute at a different time in the routine.
Prerequisites
To move a ladder diagram instruction
  • In the ladder diagram, drag the instruction to a valid drop zone:
    • If the caret appears on the Mnemonic operand, you drag the entire instruction.
    • If the caret appears on an instruction operand, you drag the instruction field
    • If you select multiple instructions, you drag all of the instructions regardless of the caret location.
      NOTE: Valid drop zones are indicated by Valid Drop Location Indicator.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal