Add an input parameter to an instruction

An input parameter provides data to an instruction. Add an input parameter to a Jump to Subroutine (JSR) or Subroutine (SBR) instruction.
Prerequisites
To add an input operand to an instruction
  1. Select a JSR or SBR instruction.
  2. Right-click the routine name and then select
    Add Input Parameter
    .
  3. In the operand for
    Input Par
    , add the tag or value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal