Close a project

Close a project when changes are complete or close a project in order to open another project.
  • On the menu bar, select
    File > Close project
    .
    TIP: If autosave is in progress, "Saving" appears in the title bar next to the project name.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal