System explorer

Use the
System
explorer
pane to view the contents of your project. The
System
explorer contains the
FactoryTalk Smart Object
s of your system. Under each
FactoryTalk Smart Object
you create the program and routine with tags and parameters created for the
FactoryTalk Smart Object
You can add programs, routines, and program or routine-scoped tags and parameters to FactoryTalk Smart Objects.
To open the System explorer, on the explorer bar, select FTDStudioSystemV1
System
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal