Specify a non-retentive assignment

The non-retentive assignment is different from the regular assignment described above in that the tag in a non-retentive assignment is reset to zero each time the controller:
  • Enters the Run mode
A non-retentive assignment has this syntax:
tag [:=] expression ;
where:
Component
Description
tag
Represents the tag that is getting the new value; the tag must be a BOOL, SINT, INT, DINT, or REAL.
[:=]
Is the non-retentive assignment symbol.
expression
Represents the new value to assign to the tag.
If tag is this data type
Use this type of expression
BOOL
BOOL
SINT
Numeric
INT
DINT
REAL
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal