Logical and Move Instructions
Use the Logical and Move instructions to perform logical operations on and move
output data.
Available Instructions
Structured Text
If you want to: | Use this instruction: |
---|---|
Sets the Q output to the state of the D input on a cleared to set
transition of the Clock input | |
Immediately update output data (the output tag of an I/O module
or a produced tag) | |
Clear or toggle the Q and QNot outputs when the Clock input
transitions from cleared to set | |
Use Set and Reset inputs to control latched outputs |
Provide Feedback