Greater Than (GT)
When enabled, the GT instruction and the operator
tests whether Source A is greater than Source B.

Available Languages
Ladder Diagram

Operands
There are data conversion rules for mixing numeric data types within an instruction. See Data conversions.
Ladder Diagram
Numeric Comparison
Operand | Data Type | Format | Description |
---|---|---|---|
Source A | SINT INT DINT LINT USINT UINT UDINT ULINT REAL LREAL | immediate tag | Value to test against Source B |
Source B | SINT INT DINT LINT USINT UINT UDINT ULINT REAL LREAL | immediate tag | Value to test against Source A |
Affects Math Status Flags
No
Major/Minor Faults
See Index through arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State | Action Taken |
---|---|
Prescan | N/A |
Rung-condition-in is false | Set Rung-condition-out to Rung-condition-in |
Rung-condition-in is true | Numeric compare: If Source A and Source B are not NANs and Source A is greater than Source B. Set Rung-condition-out to true else Clear Rung-condition-out to false. |
Postscan | N/A |
Example
Ladder Diagram

Provide Feedback