Bit Instructions

Use the bit (relay-type) instructions to monitor and control the status of bits, such as input bits or timer-control word bits.
Available Instructions
Ladder Diagram
If you want to:
Use this instruction:
Enable outputs when a bit is set
Enable outputs when a bit is cleared
set a bit
set a bit (retentive)
clear bit (retentive)
Enable outputs for one scan each time a rung goes true
set a bit for one scan each time a rung goes true
set a bit for one scan each time the rung goes false
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal