Program attributes

This table describes program attributes.
Attribute
Description
Name
The name of the program.
Parameters
(optional) Input, output, or InOut parameters of the program.
Properties
(optional) Properties of the program.
Tags
Local tags contained within this program.
Routines
Routines in this program.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal