Parameter connection examples

These examples show parameter connection syntax in the
FactoryTalk Design Studio
DSL.
Connection from one Smart Object to another Smart Object
parameterConnection myAO.program1.inParam anotherAO.program1.outParam;
Connection to a program within a controller application
parameterConnection myAO.program1.inParam controllerApp1.mainProgram.outParam;
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal