Loading
Blog
Recent ActivityRecent Activity

Why Secure Remote Access is Important for Your Brand

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Why Secure Remote Access is Important for Your Brand hero image

Remote access is increasingly common across industries – and we can easily see why. Remote access can provide significant benefits to end users and opportunities for their OEM partners.

For OEMs, remote access offers an additional revenue stream, stronger customer relationships and competitive differentiators. They can monitor a customer's machine performance from anywhere in the world and respond to critical situations remotely, saving travel and on-site costs.

End users are realizing similar benefits. They are implementing smart machines that easily integrate with enterprisewide networks and share information with their OEM partners. OEMs can respond faster to equipment issues or help prevent them in the first place – resulting in less downtime and increased production. Facility operators have fewer machines to worry about and can rely on service-level agreements to guarantee uptime.

But as end users receive more remote-access requests, they're increasingly mindful of the security implications. And with good reason – one in five manufacturers has suffered security breaches leading to intellectual property loss (source: Kaspersky Lab/B2B International). As a result, many end users' IT departments are moving toward one common platform to manage and audit all remote-access activities with vendors.

OEMs should share that concern to help protect their customers and themselves.

Lower-priced security technology can help OEMs remain competitive. However, OEMs should consider this: It only takes one hacked machine leading to an intellectual property leak, production stoppage or any other number of potential negative outcomes to ruin their reputation. Selecting a lower-level security technology may seem like a simple choice, but the wrong decision could lead to serious, long-term repercussions for an OEM's bottom line.

An unsecure remote-access connection can be an easy way into manufacturing operations, so OEMs must do all they can to secure their customers' remote-access connections and protect their own reputation.

Any remote-access solution should provide the appropriate levels of security to meet the manufacturer's current and future needs, and align with established security standards. More than that, OEMs can use security as a differentiator. An aggressive stance on protecting intellectual property, preventing unauthorized access and providing secure remote access can help OEMs stand out in a marketplace full of confusion about cybersecurity and hacking risks.

When deciding on a secure remote-access solution, OEMs have different options across a range of features and security strengths. For example, a standard level of secure remote access can provide a remote-access audit trail, on-off end-user control, outbound-only communication, secure socket layer (SSL) encryption and user authentication. More sophisticated remote-access offerings can also incorporate security certificates, MAC ID certificate, access limits by user and devices, and remote-access surveillance and notification.

Additional security benefits can be realized by using standard PLC security features with FactoryTalk® Security software. If the end user has a converged plantwide Ethernet (CPwE) architecture in place, OEMs can leverage the CPwE architecture to segment the traffic allowed through the remote-access communication. Network segmentation also allows end users to restrict access to zones within the network, protecting the end user and OEM from cybersecurity risks.

The additional cost of investing in higher security technology may seem unnecessary to OEMs. But with the correct security procedures and architectural systems in place, more secure remote access can differentiate an OEM, deliver more value to end users, and reduce the risk of a reputation ruined by cybersecurity hacks.

See how OEMs can protect themselves and their customers.

Published October 26, 2015


Sal Conti
Remote Support Manager, Rockwell Automation
Connect:
EmailEmail
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended For You

Loading
  1. Chevron LeftChevron Left Rockwell Automation Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Com... Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Blogs Chevron RightChevron Right
  5. Chevron LeftChevron Left Why Secure Remote Access is Important for Your Brand Chevron RightChevron Right
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
You can update your preferences at any time. For more information please see our {0} Privacy Policy
CloseClose