Loading
Blog
Recent ActivityRecent Activity

Best Practices for OT Firewall Management

Avoid common OT firewall errors that lead to security risks and costly downtime. Get expert tips for industrial network protection.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Teamwork professional engineer work heavy industry in factory.

Firewalls remain one of the most widely used cybersecurity measures worldwide. A 2024 Statista survey shows that about two thirds of respondents consider firewalls their main technology for protecting valuable digital assets. Yet a firewall on its own doesn’t assure true safety. When it’s misconfigured or goes without updates, it can become a glaring weakness rather than a dependable barrier. Neglected upkeep and oversight create opportunities for intruders, poking holes in what should be a strong first line of defense.

The repercussions of mismanaged firewalls can be costly in operational technology (OT) environments, where safeguarding against unplanned downtimes and employee safety are everyday priorities. Real-world incidents show just how impactful these oversights can be on operations and safety:

  • In 2023 a ransomware attack exploited weak firewall rules for a leading consumer products manufacturer, resulting in hundreds of millions in losses.
  • In 2019 poor segmentation allowed malware to spread at a leading renewable energy company, forcing the company to switch to manual operations for weeks.
  • In 2016 an improperly configured firewall let attackers steal over a decade of sensitive research data from a European aerospace corporation.

This post explores why OT firewall management demands a higher level of vigilance, what commonly goes wrong, and how to address those issues. You’ll find best practices for industrial settings and immediate steps you can take to ensure that your firewall truly defends your critical assets—rather than becoming another operational risk.

LEARN MORE ABOUT FIREWALL MANAGEMENT

Why OT Firewalls Require Special Attention

You might think IT and OT firewalls perform the same function: filter traffic, block threats, and protect key assets. But OT firewalls must handle a set of challenges unique to industrial operations. They often run in tough environments—like factories humming around the clock—and must manage specialized machine-to-machine protocols. In addition, a misconfigured firewall in OT can create weaknesses in monitoring or loss of data, which can impact compliance.

Factors that set OT firewalls apart:

Demanding Conditions
These firewalls work in hot, dirty, and noisy places. They have to be robust enough to handle dust, vibration, high temperatures, and constant operation.

Secure Network Architecture
Instead of a single, central system, industrial networks link various devices—PLCs (Programmable Logic Controllers), sensors, robots, and more. OT firewalls often create a security boundary around control systems to keep critical traffic contained.

Industrial Protocols
Many OT networks use protocols like Modbus or OPC UA, which aren’t common in IT. These protocols let machinery communicate in real time.

Avoiding Downtime
While an IT server can often be patched overnight, a production line can’t simply shut down without major consequences. As a result, patching in OT typically must wait until planned downtime. However, compensating controls, like removing, or further limiting services, can be leveraged until patching can be done during scheduled downtime.

Robust Management
OT environments require careful management due to the potential impact on production. Changes are often approved through rigorous change management processes.

Common Management Gaps
OT firewall management tends to fail when teams lack the right knowledge, skip essential updates, or fail to integrate tools that look at both IT and OT traffic. Here are a few typical issues

  • Knowledge Gaps: IT professionals may take on OT tasks without being fully trained in industrial protocols, creating incorrect rules or missing vital ones.
  • Delayed Updates: Downtime is costly, so many plants wait too long to patch firewalls, which leaves known security flaws unaddressed.
  • Weak Integration: If your OT firewall can’t exchange data with your other security tools, you risk missing threats that move between IT and OT networks.

Best Practices for OT Firewall Management

Although every industrial site is different, core principles can guide you to create a solid firewall strategy and protect production. These methods help minimize downtime, block dangerous traffic, and keep vital equipment running.

  • Start with Strong Rules
    • Default to Deny: Document and create rules for only what's needed for communications across security boundaries and deny all other traffic both inbound and outbound.
    • Segment Your Network: Isolate critical systems (like SCADA, PLCs) from less sensitive areas. This way, even if malware hits one part of the network, it can’t easily spread to another.
    • Audit Quarterly: Remove outdated or duplicate rules, which often become invisible backdoors over time.
  • Monitor and Log Wisely
    • Focus Your Logs: Track failed login attempts, big traffic spikes, and any unusual use of industrial protocols. Overlogging can create noise without adding much value.
    • Use the Right Tools: A Security Information and Event Management (SIEM) system, or an OT-specific monitoring platform, can correlate events and spot issues early.
    • Review Regularly: Logs won’t help if no one checks them. A weekly or monthly review can catch signs of trouble before they grow serious.
  • Document Every Change
    • Maintain a Rulebook: For every rule, note who requested it and why. If you can’t justify a rule’s purpose anymore, it’s time to remove it.
    • Track Timestamps and Owners: If a new rule creates problems, you need to know who added it and when.
    • Map Your Network: Keep an updated diagram of how firewalls interact with switches, routers, proxies, and other security devices. This makes troubleshooting easier and helps new team members understand the setup.
  • Build a Lifecycle Management Plan
    • Firmware Updates: Test patches in a lab if possible, then schedule them during planned downtime. Keeping your firewall firmware fresh helps close known security gaps.
    • Rule Cleanups: Review and refine your rule sets at least twice a year to remove anything obsolete.
    • Access Control Reviews: Regularly check who has rights to change firewall settings, then remove or update access for those who no longer need it.
  • Plan for Redundancy
    • Avoid a Single Point of Failure: If your main firewall fails, a backup (in an active-passive or active-active setup) should take over seamlessly.
    • Test Failovers: Routinely simulate a failure scenario in either a test environment or during an outage (i.e., safe and planned) to ensure your redundancy measures work under stress.

A well-configured firewall does more than block malware; it protects your bottom line by keeping production stable and safeguarding worker safety. As an OT professional, you know your operation’s nuances better than anyone. By combining strong rules, focused monitoring, thorough documentation, structured lifecycle management, and deliberate redundancy planning, you’ll establish a firewall strategy that meets industrial demands.

Security isn’t static—continue evolving your defenses by reviewing logs, refining access, and staying alert to new threats. The more proactive you are, the less likely you’ll face the costly fallout of a breach or unplanned downtime.

Moving Beyond Basic Firewall Rules

Standard practices—like strict rule sets, consistent logging, and frequent audits—lay the groundwork for good security. But as OT environments become more connected and threats grow more sophisticated, sometimes you need more than the basics. Here are a few advanced firewall capabilities that can help your facility stay ahead of emerging risks.

Application Filtering

Firewalls traditionally allow or deny traffic based on IP addresses, ports, or protocols. Application filtering, however, goes a step further by recognizing the actual software or services running inside that traffic. In an OT setting, this extra insight can be a game-changer because it makes sure only the specific apps your equipment relies on can pass data through the network.

  • Pinpoint Control: You get to permit only recognized industrial protocols—like Modbus or OPC UA—while blocking everything else.
  • Sharper Security: Even if attackers piggyback on typical ports, the firewall can detect anomalies that don’t match your approved apps.
  • Streamlined Bandwidth: By filtering out random or unnecessary applications, you keep network traffic focused on core production needs.

Policy Expiration

Many OT teams temporarily open firewall rules for contractor visits or special projects, but those exceptions can stay active long after everyone’s gone home. Policy expiration sets a built-in “sunset date” for each temporary rule, automatically cleaning up permissions so your firewall doesn’t accumulate unnecessary openings.

  • Reduced Oversight Gaps: You’re no longer reliant on busy staff to remember which rules need shutting off.
  • Consistent Housekeeping: Old rules and temporary credentials don’t linger as potential entry points for attackers.
  • Better Audit Trails: Each rule’s lifespan is documented, making it simpler to track when and why access was granted—and retired.

Integration with Security Tools

Your OT firewall doesn’t have to work alone. Many modern solutions link up with other security tools—like intrusion detection systems (IDS), network access control (NAC), or a Security Information and Event Management (SIEM) platform. This collective approach helps you see and respond to threats more quickly.

  • Unified View: When your firewall talks to an IDS or SIEM, suspicious activity on one system can trigger immediate action on another.
  • Faster Detection: Cross-referencing events (e.g., login attempts, odd traffic flows) paints a fuller picture of your network’s health.
  • Streamlined Response: Automated blocking or quarantining can kick in if a threat is detected, containing incidents before they escalate.

Remote Management

Industrial operations often span multiple plants or remote sites—sometimes halfway around the globe. Remote management consolidates control of all your firewalls into one central location, making updates or rule tweaks far more efficient.

  • Consistent Policies: A single team can push standardized firewall rules to every facility, rather than delegating that task to local staff.
  • Time & Cost Savings: Fewer site visits mean less downtime, reduced travel expenses, and a lower chance of on-site configuration errors.
  • Scalable Maintenance: Even if you acquire new plants or expand your operation, it’s easy to bring them online with consistent security policies.

Machine Learning & AI

While strict rule sets catch known threats, machine learning and AI are designed to sniff out anomalies—even if they’ve never been encountered before. These tools learn what typical OT traffic looks like and then raise a red flag when data patterns deviate from the norm.

  • Adaptive Protection: As your production environment evolves, so does the AI’s understanding of normal traffic.
  • Zero-Day Threat Detection: Unusual commands or data flows can trigger an alert well before a signature-based system would catch on.
  • Fewer Manual Reviews: By focusing attention on events the AI deems suspicious, human analysts can spend their time on real problems instead of sorting through routine logs.

Making the Most of Advanced Features

No single advanced feature can solve every problem on its own. Think of them more like puzzle pieces, each addressing a different angle of OT security. If your facility constantly faces vendor maintenance visits, policy expiration might provide immediate value.

Meanwhile, application filtering and OT-specific threat intelligence can help keep sabotage or malware out of your critical control systems. Decide which capabilities align best with your current pain points, test them in a controlled environment, and then roll them out more broadly once you’re confident they mesh with your operational demands.

Ultimately, these capabilities build on the core principle that firewalls in OT environments must be both secure and production friendly. When chosen wisely and configured properly, advanced features can give you the upper hand in a world where attacks are growing more inventive by the day.

Three Steps You Can Take Right Now

Even if you aren’t ready for a large-scale overhaul, a few targeted actions can quickly tighten your defensive posture. These measures won’t solve every security challenge on their own, but they can significantly reduce your exposure to common threats—and they’re simple enough to implement right away:

1. Tighten Your Rules

Trim back any sweeping permissions in your firewall policies and replace them with narrowly defined entries. Be sure to log suspicious or unusual traffic so you’ll know if something’s off.

2. Remove Dormant Accounts

Unused or shared credentials can become a silent weakness, especially in OT environments where access controls are often overlooked. Disable any accounts that no longer serve an operational need, and audit shared logins to ensure individual accountability.

3. Check Your Logs

If you notice strange outbound connections or data flows that don’t match typical patterns, investigate promptly. Not every device needs to “phone home,” and unrecognized traffic could be an early warning sign of a larger issue.

Embracing these straightforward steps sets a solid foundation for more robust security down the road. Once you’re consistently managing rules, pruning unnecessary accounts, and scanning logs for anomalies, you’ll find it much easier to layer on advanced features—like application filtering or OT-specific threat detection—without risking downtime or confusion. By staying proactive, well-documented, and alert to new threats, your firewall can evolve from a passive gatekeeper into a dynamic shield that helps protect critical processes, workers, and your overall bottom line.

Remember: Security isn’t a one-time event but a continuous cycle. By regularly reviewing your configuration, keeping a close eye on network activity, and planning updates wisely, your OT firewall can provide a strong line of defense—today and into the future.

Published February 27, 2025

Topics: Build Resilience

Michael Lester
Michael Lester
Sr. Product Security Engineer, Rockwell Automation
Michael Lester is a dedicated Senior Product Security Engineer at Rockwell Automation. Michael has over 10 years of experience safeguarding critical infrastructure. Specializing in Operational Technology (OT) infrastructure, product security, and automation, Michael has a proven track record of protecting infrastructure from electrical generation and transmission to water/wastewater and manufacturing. Holding multiple certifications including a GICSP and a degree in Computer Engineering, Michael thrives on staying ahead of evolving cyber threats, blending technical expertise with a passion for innovation to build and automate resilient systems.
Subscribe to Rockwell Automation

Receive the latest news, thought leadership and information directly to your inbox.

Subscribe now

You may also be interested in

Loading
Loading
Loading
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Com... Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Blogs Chevron RightChevron Right
  5. Chevron LeftChevron Left Best Practices for OT Firewall Management Chevron RightChevron Right
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
You can update your preferences at any time. For more information please see our {0} Privacy Policy
CloseClose