Metal Form Instructions
AVC | Name | Description |
|---|---|---|
AVC | Auxiliary Valve Control | Controls an auxiliary valve that is used with a main valve. |
CBIM | Clutch Brake Inch Mode | Used for press applications where minor slide adjustments are required, such as press setup. |
CBCM | Clutch Brake Continuous Mode | Used for press applications where continuous operation is desired. |
CBSSM | Clutch Brake Single Stoke Mode | Used in single-cycle press applications. |
CPM | Crankshaft Position Monitor | Used to determine the slide position of the press. |
CSM | Camshaft Monitor | Monitors motion for the start, stop, and run operations of a camshaft. |
EPMS | Eight-position Mode Selector | Monitors eight safety inputs to control one of the eight outputs that correspond to the active input. |
MMVC | Maintenance Manual Valve Control | Used to drive a valve manually during maintenance operations. |
MVC | Main Valve Control | Controls and monitors a main valve. |
Provide Feedback