HMI navigation for PBL

Use the
HMI Navigation
tab of the
PBL Properties
dialog box to enable or disable navigation from the HMI to input and output objects.
To enable HMI navigation to input and output objects for PBL instructions
  1. On the instruction in the routine, perform one of these actions:
    • On the Ladder or FBD instruction, select .
    • In the Structured Text editor, right-click the tag name and select
      Configure <tag name>
      .
  2. Under the
    HMI
    tab, select
    Navigation
    .
  3. To allow navigation to the input and output object from the HMI faceplate, select
    Allow navigation
    .
  4. In the
    Object tag name
    box, enter the name of the object.
  5. When online with the controller, monitor the
    Device state
    and
    Device issues
    indicators at the bottom left of the dialog box:
    • Device state
      . Displays the current device state depending on the value of the Out_Live parameter. Use the
      HMI
      tab to enter text in the
      Text to display when output equals 0
      and
      Text to display when output equals 1
      boxes.
    • Device issues
      . Displays fault conditions:
      None
      , or
      Configuration error
      .
  6. Select
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal