Complete Hookup Diagnostics and Auto Tuning

After you add and configure your modules and axes, you can download your program. After going online, you can complete hookup diagnostics and auto tuning.
To run hookup diagnostics and auto tuning
  1. To download your program, from the
    Communications
    menu, select
    Go Online
    .
    TIP: Your program can be a blank program, but it must include complete configuration information for all your modules and axes.
  2. Under the
    I/O Configuration
    folder, right-click the first motion module.
  3. Select
    Properties
    .
  4. Decide on the appropriate button to select:
    If:
    Then:
    You assigned your axis to channel 0
    Select the button next to the Channel 0 field
    You assigned your axis to channel 1
    Select the button next to the Channel 1 field
  5. Select the
    Hookup
    tab.
  6. Run the hookup diagnostics. For more information about hookup diagnostics, see the ControlLogix Motion Module User Manual.
  7. Select the
    Tune Servo
    tab.
  8. Run auto tuning. For more information about auto tuning, see the ControlLogix Motion Module User Manual.
  9. When diagnostic testing and auto tuning are complete, select
    Finish
    .
  10. For each axis, repeat steps 4 through 9.
  11. For each module, repeat steps 2 through 11.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal